Logo von amplify - The Pepperl+Fuchs Magazine

November 15, 2017

The BlueBeam Group

BlueBeam, an innovative technology developed by Pepperl+Fuchs, offers a unique level of precision for rotary encoders: a blue LED combined with a high-performance scanning chip enables optimal use of light.

In the light of day, the cool blue glow in the metal interior of the opened-up device is hardly noticeable. Only under closer scrutiny can its origin be recognized: a focused light beam, only about the size of a pinhead. The considerable impact of this small blue point is, however, not to be dismissed: “Phase position A:B is far below 10%,” states Matthias Padelt, specifically quantifying the effect of the new “BlueBeam Technology.” As Managing Director, he is responsible for Pepperl+Fuchs Drehgeber GmbH. When you talk to Padelt and his team—Head of Innovation Management Thorsten Gippert and Head of Product Management Stefan Horvatic—it is easy to see how much lifeblood has flowed over the past few months into the ENI58IL series, the first to use BlueBeam technology. Horvatic points with a pen to the open incremental rotary encoder in front of him: “With this, we are setting a new standard in the market in terms of signal quality.”

Insight into the technology of ENI58IL series rotary encoders with innovative BlueBeam technology

The ENI58IL series with innovative BlueBeam technology

Blue Trumps Red

The team achieved this by implementing a blue emitter LED and the corresponding receiver diodes. When used in conjunction with a powerful sensing chip, a significantly better utilization of light is possible than with commonly used infrared technology. But there were some hurdles that had to be cleared along the way.
Gippert recalls: “Selecting the optimal sensing chip, for example, was no easy task. We spent so much time researching until we found a model that met our requirements exactly.” The result of their effort is a higher resolution and greatly improved signal amplitude, as well as reduced jitter.
To further increase the extremely high measuring quality achieved with BlueBeam technology, the adjustment of the code disc was also refined in comparison to the standard procedure. “With the ENI58IL series, we´re moving in a new direction: here, the precise insertion of the disc is checked on a microscopic level during the manufacturing process. This step leads to improved absolute accuracy for applications in which even the smallest deviations cause a noticeable loss of performance—for example, when ensuring the perfect blade alignment on a wind turbine,” says Padelt, outlining the benefits.

Delicate Technology, Interlocked

In this context, it is not surprising that, during development, the team also worked intensively on the issues of longevity and process reliability. Along with the EMC protection circuit, this is supported by the robust construction with interlocked bearings that withstand high loads and prevent the ball bearing from being crushed. In addition to this powerful interlocking, the delicate BlueBeam technology has a positive impact on process reliability. “With BlueBeam, signals remain stable under high mechanical force such as shock or vibration, as high-frequency scanning offers more tolerance toward such interference,” explains Horvatic about the welcome side effect of the innovation.

Matthias Padelt, Thorsten Gippert and Stefan Horvatic in the production hall

Matthias Padelt, Managing Director Pepperl+Fuchs Drehgeber GmbH // Thorsten Gippert, Head of Innovation Management // Stefan Horvatic, Head of Product Management (left to right)

Sophistication Comes Standard

Is ENI58IL an exclusive series only for extremely demanding applications? Gippert forcefully denies this: “Quite the contrary! We provide the features needed for high-performance applications in a series of rotary encoders for the broad market. In doing so, we can handle applications with a sophisticated standard rotary encoder that previously could only be achieved using specialist devices. This is also reflected in the breadth of the available portfolio. We have almost all types of shafts, flanges, and connections.” Horvatic adds: “With ENI58IL, users receive innovation and reliability as standard worldwide, even in the smallest quantities.”
After the last steps of the product launch are taken, the question that remains for the three managers is: What´s next on the agenda? Padelt barely hesitates: “For now, we are eager to hear how this series of rotary encoders is received by our customers. At the same time, we are moving on to new challenges. This much is clear: BlueBeam technology will also be used in future product developments.”

Learn more

By |2025-06-12T09:09:41+00:00November 15, 2017|Technologies + Innovations, Company Insights, Industrial Sensors|Comments Off on The BlueBeam Group

15. November 2017

The BlueBeam Group

BlueBeam, eine innovative Technologie von Pepperl+Fuchs, bietet einzigartige Präzision für Drehgeber: Eine blaue LED in Kombination mit einem leistungsstarken Abtastchip ermöglicht eine optimale Ausnutzung des Lichts.

Bei Tageslicht ist der kühle blaue Schimmer im metallenen Inneren des aufgeschraubten Gerätes kaum wahrnehmbar. Erst bei näherem Drehen und Wenden erkennt man seinen Ursprung — einen fokussierten, gerade einmal stecknadelkopfgroßen Lichtkegel. Die beachtliche Wirkung dieses kleinen blauen Punkts ist jedoch nicht von der Hand zu weisen: „Phasenlage A : B weit unter 10 %“, so konkret beziffert Matthias Padelt den Effekt der neuen „BlueBeam-Technologie“. Als Geschäftsführer verantwortet er die Pepperl+Fuchs Drehgeber GmbH. Im Gespräch mit ihm, Leiter Innovationsmanagement Thorsten Gippert und Leiter Produktmanagement Stefan Horvatic ist deutlich spürbar, wie viel Herzblut in den vergangenen Monaten in die Baureihe ENI58IL geflossen ist, in der die BlueBeam-Technologie nun zum ersten Mal zum Einsatz kommt. Horvatic deutet mit einem Stift auf den vor ihm liegenden, geöffneten Inkremental-Drehgeber: „Damit setzen wir am Markt einen neuen Maßstab in Sachen Signalqualität.“

Blick in das technische Innenleben ENI58IL mit BlueBeam-Technologie

Die neue Baureihe ENI58IL nutzt die BlueBeam-Technologie.

Blau sticht Rot

Gelungen ist dies dem Team über die Implementierung einer blauen Sende-LED und der entsprechenden Empfangsdioden. Im Zusammenspiel mit einem leistungsstarken Abtastchip ist so eine deutlich bessere Ausnutzung des Lichts möglich als mit üblicherweise verwendeter Infrarottechnologie. Auf dem Weg dorthin mussten jedoch einige Hürden genommen werden.
Gippert erinnert sich: „Den passenden Abtastchip auszuwählen war zum Beispiel kein einfaches Unterfangen. Da ist einige Zeit in die Recherche geflossen, bis wir ein Modell gefunden hatten, das genau unseren Anforderungen entsprach.“ Das Resultat der Mühen sind jetzt, neben dem verringerten Jitter, eine höhere Auflösung und stark verbesserte Signalamplitude.
Um diese dank der BlueBeam-Technologie erreichte enorme Messqualität noch weiter zu steigern, wurde auch die Justierung der Codescheibe gegenüber den üblichen Verfahren verfeinert. „Bei der Baureihe ENI58IL gehen wir einen neuen Weg: Hier wird das präzise Einsetzen der Scheibe während des Fertigungsprozesses mikroskopisch überprüft. Dieser Arbeitsschritt führt zu einer verbesserten absoluten Genauigkeit von Anwendungen, in denen schon kleinste Abweichungen spürbare Leistungsverluste nach sich ziehen — etwa bei der idealen Ausrichtung eines Rotorblatts an einem Windrad“, umreißt Padelt die Vorteile.

Verblockte Filigrantechnik

Vor diesem Hintergrund überrascht es nicht, dass sich das Team während der Entwicklung ebenso intensiv mit den Themen Langlebigkeit und Prozesssicherheit beschäftigte. Dafür spricht neben der EMV-Schutzbeschaltung der robuste Aufbau mit einer verblockten Lagereinheit, die dauerhaft hohe Lagelasten verkraftet und ein Auspressen der Kugellager verhindert. Neben dieser wuchtigen Verblockung zieht jedoch auch die filigrane BlueBeam-Technologie positive Effekte für die Prozesssicherheit nach sich. „Mit BlueBeam sind die Signale unter mechanischen Einwirkungen wie Stößen oder Vibrationen gleichbleibend hoch, da die hochfrequente Abtastung mehr Toleranz gegenüber solchen Störeinflüssen bietet“, erklärt Horvatic den willkommenen Nebeneffekt der Innovation.

Matthias Padelt, Thorsten Gippert und Stefan Horvatic in der Produktionshalle

Matthias Padelt, Geschäftsführer Pepperl+Fuchs Drehgeber GmbH // Thorsten Gippert, Leiter Innovationsmanagement // Stefan Horvatic, Leiter Produktmanagement (von links nach rechts)

Stark in Spitze und Breite

Handelt es sich bei ENI58IL demnach um eine exklusive Baureihe ausschließlich für extrem anspruchsvolle Applikationen? Gippert verneint das energisch: „Ganz im Gegenteil — wir packen das Leistungsvermögen für hochperformante Anwendungen in eine Reihe von Drehgebern für den Flächeneinsatz. Wir decken also mit einem ausgeklügelten Standard-Drehgeber Szenarien ab, die bisher nur mit speziellen Geräten zu lösen waren. Das zeigt sich auch in der Breite des Portfolios. Wir verfügen hier über nahezu alle Typen von Wellen, Flanschen und Anschlüssen.“ Horvatic ergänzt: „Mit ENI58IL erhalten Anwender Innovation und Zuverlässigkeit serienmäßig, weltweit und selbst in kleinsten Stückzahlen.“ Nachdem die letzten Etappen des Produkt-Launchs genommen sind, bleibt die Frage an die drei, was als Nächstes auf der Agenda steht. Padelt muss nicht lange zögern: „Jetzt sind wir erstmal gespannt, wie unsere Kunden diese Drehgeberreihe annehmen. Parallel geht´s weiter zu neuen Herausforderungen. So viel lässt sich schon sagen: Die BlueBeam-Technologie wird sicher auch für kommende Entwicklungen eingesetzt werden.“

Mehr zum Thema

By |2025-06-12T09:16:09+00:00November 15, 2017|Industrielle Sensoren, Technologien + Innovationen|Comments Off on The BlueBeam Group
Go to Top